cancel
Showing results for 
Search instead for 
Did you mean: 

Maximum Output capacitance for STBB3JR. What is the recommended upper limit cor ceramic capacitors?

HDono.1
Associate
 
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @HDono.1​, to the community!

There is only a recommended minimum of 10µF for both the input and output capacitors, which should also be ceramic because of the lower ESR.

What capacitance would you want to use?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.