cancel
Showing results for 
Search instead for 
Did you mean: 

L9961 - not using VREG advice

KrauseRobotics
Associate

Hi all,

I am looking at using the L9961 (https://www.st.com/en/power-management/l9961.html) for a project and after looking at the datasheet, I see it has it's own LDO.

The LDO can supply up to 35mA (pg. 13 of the data sheet). My design will use a STM32F103C6, which can use up to 150mA, plus I will have additional peripherals that will consume more.

My plan is to use a standard TPS692910-Q1 from TI to provide power for my 3v3 rail, as it can supply up to 1A of current which is plenty.

My question is, how do I handle not using the internal LDO on the L9961? It seems like the datasheet has all the IO referenced to the VREG coming from the LDO, and of course, I will have my own. 

 

Thanks,

Chad

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KrauseRobotics
Associate

I should note that I am a bit of a rookie when it comes to PCB and electrical design - I am software engineer by trade, so apologies if my question seems stupid or simple

PCOLE.1
ST Employee

Hi,

if the VREG is not used, its capacitor shall be left mounted and you may add 10Mohm resistor as load.

Ciao,

Piero