cancel
Showing results for 
Search instead for 
Did you mean: 

L9369: SPI interface questions

FTCGIE
Visitor

Hi,

Good day,

May we seek your expertise for the following inquiry:

1. What is the SPI frame format for L9369 RT?
2. Is it configurable via SPI?
3. What is the default SPI frame configuration for L9369 RT?

Thank you.

1 REPLY 1
Peter BENSCH
ST Employee

You have already opened a ticket with the number 00262344 (internal number) in parallel with the personal Online Support OLS for this request, so the response from the colleagues should be awaited. If you have an urgent need, you should contact your local distributor.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.