cancel
Showing results for 
Search instead for 
Did you mean: 

L6474 overheating

estie
Associate II
Posted on September 08, 2015 at 12:52

I am using three L6474s to drive NEMA23 format motors.

Using the default register configurations the chips are rapidly getting very hot and causing a TH_WRN condition.

I found a post here that stated that the default config caused high frequency switching which produced ''strong'' heat dissipation. It also recommended some alternative configuration, the main change of which was reducing TON_MIN from 4 µs to 4µs . There was also suggest that some configurations lead to the control algorithm being unstable.

I did that and reduced slew-rate and now the chips are getting to a much more reasonable circa 70 deg. C.

while this did provide a convenient opportunity to test my ISR handling a FLAG input change, it seems odd that the chip is not supplied with a better default configuration.

What kind of motor loading is the default config suitable for?

Now with about six configurable parameters for internal algorithm, my semi-arbitrary set of values seems more of a hack than an engineered solution.

Is there any guidance on how to tune these parameters to reduce dissipation and avoid possibly unstable configurations?

Thanks.

0690X0000060MoYQAU.gif

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0