cancel
Showing results for 
Search instead for 
Did you mean: 

L6472 and the ABS_POS register

james239955
Associate
Posted on December 04, 2014 at 00:32

Hello, 

I have a design using several L6472 ICs.  Everything seems to work fine except when I go to read the abs_pos register.  For instance: if the position register is reading 0x00084AF and I command the driver to move the motor 400 half-steps (bi polar motor and half stepping) I get a full revolution of the motor but when I read the abs_pos register after the move it reads 0x00086BF.  A change of 528.  If I tell the driver to move another 400 half-steps in the same direction and then read the abs_reg again it reads 0x00087CF.  A change of 272.  It is odd that the sum of the differences is 800.  Am I missing something basic here?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gigi
ST Employee
Posted on December 12, 2014 at 12:26

Ciao

Regarding xSpin family question I suggest to ask in this forum

Home STe2eCommunities > Motor Control > Motor Driver ICs and Boards

Ciao

Gigi