cancel
Showing results for 
Search instead for 
Did you mean: 

L5970AD DCDC schematic doubt

AlexMachine
Associate II

Hello,

I am investigating in using L5970AD DCDC converter for a 12VDC to 3V3 need.

It was advised to me by the ST DCDC online simulator.

It's a 20 year old circuit but it it matches the budget, the additional BOM and the efficiency so I am interested.

But I don't reach in answering some questions. If one of you can share some return of experience about this chip I am gladly listening.

I am in design phase, looking datasheets, and except error I don't find my answers :

- The VREF signal is noticed as 3V3. 3V3 is the output I want to create. On the Typical application schematic it seems not clear for me if connecting VREF to the output is okay, or if we need a precursor 3V3 ??? Should we supply a high impedance 3V3 from resistor divided input for example ? I couldn't reach advise about it, the is no paragraph about VREF. Is it an input or an output? What about generating 5V, do we need a 3V3 rail ?

 

Also, even if switching frequencies are different, why not group L5970AD and L5970D in one unique datasheet ?

 

Thank you for reading,

A++ Alex

 

AlexMachine_0-1729210148466.png

 

26 REPLIES 26
AlexMachine
Associate II

It may be a PGOOD pin for LED

Yes VREF in the air

One book "Fundamentals of Power Electronics" is very good.

Author s R. W. Erickson

Depends, because high frequency is more loss in semiC no?

Interesting to separate spectrums from supply EMI and low freq app like audio, to ease filtering.

For L5970 SYNC must be <3V3.

But this 3V3 is the fifth weel of the charette.

PGOOD

What shows the app note?

Regards

Ok thank you for sharing.

Waiting for @Peter BENSCH insight.

Happy to read you

 

No, the mark as Accept as solution was set by yourself, you can also reset it with “Not the Solution”.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

It's a bit too mixed up for me. Which question is currently open?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.