2021-05-23 06:57 PM
Hi,
Is it possible to force STUSB4500 to operate at 15V using only hardware solution and don't require any NVM programming?
Thank you
2021-06-02 11:28 PM
This is not possible.
The STUSB4500 is pre-programmed in factory to accept 3 possible power profiles by default: 5V, 15V, 20V. (refer to datasheet)
If you want a different configuration, then it is mandatory to reprogram the NVM memory once.