cancel
Showing results for 
Search instead for 
Did you mean: 

In the SPI protocol of L9305, how is the cnt bit of bit21 used

ryze_bai
Associate

Hi,

There is no specific writing description for the cnt bit in the manual.I guess it's the first time I've powered on and written 1.

If I reset the chip through the reset pin, should the cnt be written to 1 after the reset or keep the negation of the last write?

Thanks.

0 REPLIES 0