cancel
Showing results for 
Search instead for 
Did you mean: 

I need a help to identify this part

Proboszcz
Associate II

Hello!

 

I have two components (in SMB package probably).

 

The markings are:

1) ME G3 202 (no polarity stripe on package)

ME G3 202.png

2) EE G3 223 (with polarity stripe)

EE 63 223.png

Can you help me decipher what these elements may be and what may be the difference between ME and EE and the fact that one has polarity stripe and the other does not?

 

Regards

C. Jones

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

ME = SM6T18CA (bidirectional)
EE = SM6T18A (unidirectional, same data sheet)

The unidirectional TVS has a unique polarity, which is why its cathode is marked with a dash/bar. The bi-directional one is electrically symmetrical and can be installed with any polarity.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

ME = SM6T18CA (bidirectional)
EE = SM6T18A (unidirectional, same data sheet)

The unidirectional TVS has a unique polarity, which is why its cathode is marked with a dash/bar. The bi-directional one is electrically symmetrical and can be installed with any polarity.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Proboszcz
Associate II

Great! Thanks a lot!