cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STBB2J-30 to power up my system, and finding that on start-up, the Vout ramping up in step and a few current spikes on Vin.

AStri.1
Associate

I thought it was because of the capacitive load (25uF), so I tried to reduced it to 15uF, but haven't gotten any changes. I tried also to reduce the slew-rate on Vin, still no significant difference. Is this because of the soft-start?.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0