cancel
Showing results for 
Search instead for 
Did you mean: 

HVLED815PFTR-based LED Driver minimun load

alvaro
Associate
Posted on March 03, 2014 at 13:59

Hi,

I am involved in the design of a LED driver based on the HVLED815 IC. It works great with a load greater than 4W, but LEDs start blinking if the load is less than 3W (approx). So, my question is if there is any minimun load required to get a constant current output, or if it is just a dimensioning problem.

Any commnet will be appreciate. Thanks in advance.

Best regards,

#hvled815 #led-driver #light-load
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0