cancel
Showing results for 
Search instead for 
Did you mean: 

Hold current setting L6472

Rein van der Zee
Associate
Posted on April 19, 2017 at 11:00

Hello,

I'm using the EVAL6472H evaluation kit to experiment with the L6472 driver. I'm having trouble with the hold current setting, when is set the hold current to 200 mA for example, only 70 to 100 mA flows through the motor. When i use a higher current setting, more current will flow through the moter. The current flowing through the motor even exceeds the limit, a setting of 500 mA results in a current flow of about 900 mA. 

I checked the TVAL_HOLD (address: 0x09) and it contains the correct, previously written value.

I hope someone can point me in the right direction.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Enrico Poli
ST Employee
Posted on April 26, 2017 at 14:59

What about the other parameters of the current control algorithm?

Posted on May 01, 2017 at 08:02

Hello,

Thanks for your answer.

I already figured it out, there was a problem with the SPI communication and everything is working normally now.

Best regards,

Rein