2020-07-07 4:50 AM
The circuit is intended to recharge a NiMH battery, with a input voltage (Vin) of 15V.
Using Rsense in series with the inductance I have a maximum output voltage (Vout) of Vin - 1.5V.
If instead Rsense refers to GND, I can reach 100% dc.
This behavior persists even in the "no load" condition with Vref << 1.235V ,
So I would like to understand if it's possible to limit the current by using Rsense in series with inductance and have dc=100%
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.