cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am currently using a STP16CPC26, and due to supply shortage,we would like to replace it. the STP16CPC05 seems a good fit, but I can't really find the differences with the PC26, except for current output (90mA vs 100mA), could you help me ? Thanks

MNEDE.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @MNEDE.1​, to the community!

Yes, the newer STP16CPC05 can replace the older STP16CPC26 and contains some improvements that make component selection easier (smaller bypass capacitor possible) or the slightly higher maximum driver current.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @MNEDE.1​, to the community!

Yes, the newer STP16CPC05 can replace the older STP16CPC26 and contains some improvements that make component selection easier (smaller bypass capacitor possible) or the slightly higher maximum driver current.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MNEDE.1
Associate

Hi Peter,

Yes thank you very much for the quick answer.

Have a nice day,

M.NEDELEC

You're welcome!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck and regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.