cancel
Showing results for 
Search instead for 
Did you mean: 

Hi , about the VN9008AJ, do I have to connect the power tab to the ground?

VLAVI.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The confirmation comes late, but may still be interesting for later readers: yes, the bottom slug is the VCC connection, often connected to VBAT. Unfortunately, this was neglected to be mentioned or labelled in the data sheet, but in the data brief of the comparable EV-VN9007AJ it can be recognised with pin number 0.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
salmazan
Associate

I have been reading all the information and although is not so clear, the power tab is the only option to connect Vcc.

Peter BENSCH
ST Employee

The confirmation comes late, but may still be interesting for later readers: yes, the bottom slug is the VCC connection, often connected to VBAT. Unfortunately, this was neglected to be mentioned or labelled in the data sheet, but in the data brief of the comparable EV-VN9007AJ it can be recognised with pin number 0.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.