2021-09-29 5:38 AM
2021-09-29 6:12 AM
Welcome, @Torsten Röder, to the community!
which UL certification do you expect?
Regards
/Peter
2021-09-29 6:20 AM
Something like an e-file number, such as E354278 for STMPS2151. I can't find the component on the UL pages.
2021-09-29 6:21 AM
I can't find the component STMPS2252TTR on the UL pages
2021-09-29 6:31 AM
Have you got an URL where you've found STMPS2151 on the UL pages?
Regards
/Peter
2021-09-29 6:40 AM
2021-09-29 7:08 AM
No, there are currently no plans to carry out UL certification for the STMPS2252 as well.
With a corresponding project size, this can be taken into account, please contact your preferred distributor.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-09-29 7:13 AM
What does this mean in numbers "corresponding project size"?
2021-09-29 7:43 AM
Well, it has to be taken into account that such certification cannot be obtained free of charge from UL. For this reason, it is recommended that you explain the need for such certification in a direct discussion with us or through your distributor.
Regards
/Peter
2021-09-29 10:57 PM
We need this chip as a replacement for the TI variant TPS2052BDGN. This component is UL-recognized and we use the component in our devices, which themselves have UL approval. If components have to be replaced in such devices, a declaration to UL regarding a change is easier if this replacement is already listed with UL. If that is not possible, then we have to find another replacement.
Best regards,
Torsten Röder
Translated with www.DeepL.com/Translator (free version)