cancel
Showing results for 
Search instead for 
Did you mean: 

G86 Diode need data

dsgn
Associate II

dsgn_0-1729866093466.jpeg

 

3 REPLIES 3

Earlier post, you don't need to post things three times.

https://community.st.com/t5/other-hardware/diode-g86-need-data/td-p/735765

Marking hard to read, is the second diode on the board the same?

Are we sure these are authentic? marking look awfully rough

@Peter BENSCH 

ST DIODE 68B

ST DIODE G8B

 

Wrong style for BZW50-68B axial

Perhaps SM15T68A ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

It’s really hard to read, but it is GB6 = STPS1L60A, a Schottky in SMA.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Good morning.

I apologize for the delay, have tried and it is not working.

it should start clipping at approximately 82 volts according to a unit that is still working

Thank you

Denis Norton