2019-05-07 1:03 AM
when:
VDD=SD=IN=PWM=12V
Voltage between OUT1 and OUT2 is +40mV
Direction of OUT1-OUT2 voltage flips depending on DIR
This happens when driver supply voltage (VS) is disconnected or VS = 12V , 24V, 48V .
I'm guessing that the output driver of PWD5F60 is similar to N-channel 600 V, 1.38 Ohm typ., 3.5 A MDmesh DM2 Power MOSFET in STD5N60DM2. So Vs=48V should be sufficient for saturation.
I have a couple of EVALPWD5F60 parts with same response.