2024-07-17 11:16 PM - last edited on 2024-07-18 5:15 AM by Peter BENSCH
Dear Sirs,
Could you advise me dynamic resistance(Rd) of TVS such as SM6T33CAY used to clamp against pulse 5B per ISO 7637-2 or load dump B in ISO 16750-2.
Its voltage source waveform is clamped instead of exponential surge curve.
Thanks
John
2024-07-29 2:33 AM
Welcome @JMan, to the community!
The question should be answered as you have already connected with your local contact so this thread can be closed?
Regards
/Peter