cancel
Showing results for 
Search instead for 
Did you mean: 

Driving a proportialnal hydraulic valve with VN5E050?

henrik239955_stm1
Associate II
Posted on August 06, 2014 at 11:43

Hello

I would like to control a hydraulic valve (24V, 0-2.6A) proportional (0-100%) with a PWM signal from a MCU. I need to measure the current, detect open loop and short detection to VCC.

I found the VN5E050J-E, but I'm not sure it can handle PWM as the datasheet says nothing about maximum switching frequency. Would 20 kHz PWM be ok?

Is there a better choice than VN5E050 for driving a proportional hydraulic valve (24V, 0-2.6A)? Maybe there is an IC with a h-bridge solution to eliminate power loss of the diode? Any suggestions are appreciated!

Henrik
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0