cancel
Showing results for 
Search instead for 
Did you mean: 

drive the motor using STM32fr07vg

vinothraj
Associate II
Posted on December 20, 2012 at 13:56

Hi,

   i am trying to drive the motor using stm32f407vg. 

So i use the example code for this project from :

\STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Project\STM32F4xx_StdPeriph_Examples\TIM\6Steps.

i changed the code little.(from 6 channel from 4 channel).i am bit confused to use in timers and pwm.

but i could not get the desired result in oscilloscope  from my attempt . 

i want the result like attachment in this post.which example will i use? 

any suggestion...
0 REPLIES 0