cancel
Showing results for 
Search instead for 
Did you mean: 

Communication issue with L9961

rizwan99
Associate II

can someone help me with communication of l9961 chip to get voltages of 4s cells n current n charge accumulated by using esp32 or aurdino i dont have this chip n i am not a coder i tried my best but can get any data from the chip just i2c add 0x49 n this register 0x00 gives  0x41 n nothing please hep

1 REPLY 1
KTANG.9
ST Employee

Hi,

The STM32 + L9961 project is available on ST website - https://www.st.com/en/embedded-software/stsw-l9961bms.html

You can import this with STM32 CUBE IDE.

You can look at how it is done in the code. 

 

SoC example using AEK_POW_BMS63EN ( L9963E ) .

This example is based on 14 x Li-ion battery cells LG INR 18650 MJ1.

https://www.aboutenergy.io/stmicroelectronics-model-download

ST has a SoC example using AEK_POW_BMS63EN ( L9963E ) .

This example is based on 14 x Li-ion battery cells LG INR 18650 MJ1.

 

Lemberg solutions using SPC58 E Line MCUs + L9963 14 Cells BMC IC Evaluation Board and a 4 cell pack for 18650 batteries.

https://lembergsolutions.com/blog/battery-state-charge-explained-soc-algorithm-setup-example