cancel
Showing results for 
Search instead for 
Did you mean: 

Can the X-NUCLEO-IHM08M1 board withstand a load of 360W at 15A and 24V?

FBomb
Associate

Hi everybody,

as the title states, I was wondering whether the X-NUCLEO-IHM08M1brushless motor driver can withstand the described load for long periods of time.

The board is rated for 15ARMS and the voltage is in the functioning range, so I think it should be ok with that.

The reason I am in doubt is that, looking on the internet for similar drivers, they all have big heat sinks, while this board has no visible heat sink (at least from the images I saw).

I don't know if this can help, but the load I'm talking about is an e-bike motor. The controller that comes with it is rated for the same voltage and current values I wrote.

Thank you very much for your attention.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0