cancel
Showing results for 
Search instead for 
Did you mean: 

L6229 L6235 +5V Supply

dgrimes
Associate II
Posted on December 03, 2014 at 19:24

For EVAL6229 or EVAL6235 with PractiSpin board it looks like 3.3V or 5V reference is from other PCB, is there a way for L6229 or L6235 to supply 5V (for EN, F/R, BRAKE) internally?

Does ST make compatible 8-52V to 5V (or 3.3V) DC-DC conveter that would be good companion for L6229 if this cannot make own 5V source (like L4971 but with fixed output and not needing so many external components?)
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Enrico Poli
ST Employee
Posted on December 15, 2014 at 16:07

The EVAL boards can generate the 5V pull-up voltage through a zener diode.

For your final application ST proposes a wide range of step-down converters covering the 8V to 52V range. For example you can use the

http://www.st.com/web/catalog/sense_power/FM142/CL1456/SC355/PF63210

,

http://www.st.com/web/catalog/sense_power/FM142/CL1456/SC355/PF63207

and

http://www.st.com/web/catalog/sense_power/FM142/CL1456/SC355/PF63205

.