cancel
Showing results for 
Search instead for 
Did you mean: 

Can STEF01 handle negative transients (350 ms) of -40 Volt?

PradipRaj
Associate

we want to know that. Can this IC E-Fuse capable to handle negative transients (350 ms) of -40 Volt.

Please Reply ASAP.

MPN: STEF01

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

@PradipRaj 

If you are asking about a possible negative input voltage: reverse polarity protection is required for this, e.g. with a p-channel MOSFET and at -40V also a TVS or zener to limit the voltage to the maximum gate voltage. Such reverse polarity protection blocks the negative voltage and thus prevents the destruction of the downstream components, in this case the STEF01.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
TDK
Super User

On the output pin? The output pin is limited to -0.3 V. -40 V is far outside of these bounds. Operation outside of the absolute maximum ratings is not guaranteed.

TDK_0-1758031947253.png

 

If you feel a post has answered your question, please click "Accept as Solution".

@TDK wrote:

Operation outside of the absolute maximum ratings is not guaranteed.


Indeed.

@PradipRaj Worse than that - operation beyond the Absolute Maxima may cause damage:

AndrewNeil_1-1758032284814.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

And in this case, will almost certainly cause damage.

The -0.3 V limit suggests protection diodes. When you try to pull a net to - 40 V, those diodes will activate and try to bring VSS to - 40 V. That in turn will almost assuredly bring other rails down.

If you feel a post has answered your question, please click "Accept as Solution".
Peter BENSCH
ST Employee

@PradipRaj 

If you are asking about a possible negative input voltage: reverse polarity protection is required for this, e.g. with a p-channel MOSFET and at -40V also a TVS or zener to limit the voltage to the maximum gate voltage. Such reverse polarity protection blocks the negative voltage and thus prevents the destruction of the downstream components, in this case the STEF01.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.