cancel
Showing results for 
Search instead for 
Did you mean: 

advice on starting with high inertia

jneely
Associate II
Posted on July 02, 2003 at 07:31

advice on starting with high inertia

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
maxime2399
Associate II
Posted on May 17, 2011 at 10:16

You should probably try to increase the starting torque by increasing the starting current (the torque is proportional to the current).

If this is not helping or if you reach the maximum current capability of your system you will probably have to use a slower starting ramp.

The inertia is limiting the acceleration of your motor
jneely
Associate II
Posted on May 17, 2011 at 10:16

Is there a way to adjust the starting torque of the motor controller when using a load with a high inertia? For example, I am using a 24v motor connected via a direct drive shaft to an alternator. The motor will start up without the alternator. However, when the alternator is connected, the motor tries to start, but starts and stops repeadedly. Is there any advice on trying to a start a motor with high interia?

Thanks.