cancel
Showing results for 
Search instead for 
Did you mean: 

AC?DC conversion system

AKerm.1
Associate

Dear all

I would like design a circuit for AC/DC conversion of a 3 phase AC voltage with different frequency and different amplitude. The input power of the circuit can be changed form 4W up to 300W. Actually, circuit input is generated by a output of a 3 phase generator which is linked to a small wind turbine, so its frequency and output voltage varies considerably. Maximum output voltage is about 36v.

I appreciate it if you instruct me for using the ST parts (power modules) similar to VIPER31.

Best regards

Amin

1 REPLY 1
AScha.3
Chief III

Hi,

Here you can find helping hands for your project:
 
 
If you feel a post has answered your question, please click "Accept as Solution".