2004-09-07 9:14 PM
2011-05-17 1:17 AM
dear sir,
I want to drive a bldc motor in sensorless mode with st7mc. but because I use IR2103 as driver now I have to change the source code. Now I want to know if there are any other places I have to change the source code except for MPOL and MPWME? best regards, mcuinterest2011-05-17 1:17 AM
Hi,
ok to change MPOL register due to the fact that the low side input of the driver is active LOW. But, it isn't clear for me why you have to manage also the MPWME register? Waiting your answer, Tanio