About 440VAC to DC converter
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-02-14 7:41 PM
Posted on February 15, 2015 at 04:41
Hi, I got some information about VIPer06 from google search, it can be applied for 440 VAC input, but the drain current is only 350mA, my requirement is greater than 2A, in ST web site, if I choose VIPer100A-E, does this component can be applied for 440 VAC input ?
Additionally, according to the datasheet of VIPer100A-E, it showed as below : ''Typical applications cover offline power supplies
with a secondary power capability of 50W in wide
range condition and 100W in single range or with
doubler configuration
'' Does it mean the maximum output power is 100W only ? my requirement is 140W DC output, anyone can help me ? thanks !
Labels:
- Labels:
-
AC-DC Conversion
0 REPLIES 0