cancel
Showing results for 
Search instead for 
Did you mean: 

a question about function u8 SVPWMEOCEvent(void) of FOC control based on the stm32

1835116269
Associate II
Posted on June 12, 2014 at 12:26

       I? recently? doing the FOC control program based on the stm32 .  

 

      single shunt resistor.

 

      ''

Return false after first EOC, return true after second EOC

'' in the introduction of functions about 

u8 SVPWMEOCEvent(void)  .However?When the ADC sampling end for the first time

??When the ADC sampling for the second time??

 

function prototype?

                  

/*******************************************************************************

* Function Name  : SVPWMEOCEvent

* Description    :  Routine to be performed inside the end of conversion ISR

                        store the first sampled value and compute the bus voltage and temperature

                        sensor sampling  and disable the ext. adc triggering.

* Input           : None

* Output         : Return false after first EOC, return true after second EOC

* Return         : None

*******************************************************************************/

u8 SVPWMEOCEvent(void)

{

  if (bDistEnab == 1)

  {

    // Diabling the Injectec conversion for ADC1

    ADC_ExternalTrigInjectedConvCmd(ADC1,DISABLE);

  }

  // Store the Bus Voltage and temperature sampled values

  h_ADCTemp = ADC_GetInjectedConversionValue(ADC2,ADC_InjectedChannel_1);

  h_ADCBusvolt = ADC_GetInjectedConversionValue(ADC2,ADC_InjectedChannel_2);

  return ((u8)(1));

}

#foc-single-shunt-resistor
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0