2025-06-26 9:58 AM - last edited on 2025-12-29 11:28 AM by ELABI.1
Hi All,
I am choose the STM32U585VIT6 MPU to design our customized board. Firstly I design a simple basic connection to program it and only blink the LED for confirmation our initially circuit. Also I following the AN5373 document.
When I flash the code getting the error below
Error in initializing ST-LINK device.
Reason : No device found on target.
Find the attached schematic.
Please guide me what is the issue and how to resolve it.
2025-06-26 11:03 AM
Is the chip powered?
Try to connect with STM32CubeProgrammer. If unsuccessful, show a screenshot.
Schematic looks fine.
2025-06-26 8:32 PM
It's an MCU, not an MPU, like an embedded Linux STM32MP device.
ST-LINK reports voltage correctly, Pin 1 or 2 should be VTarget for the pin drivers to work.
Check with STM32 Cube Programmer
2025-06-27 2:33 AM
Hi,
Yes chip is powered 3V3 externally and all the ground are common. I already try many times to program the chip using ST-LINK V2 and ST-LINK V2 IOSL but getting the same error shown in shared image.
Also I shared screenshot.
Thanks.
2025-06-27 2:40 AM
2025-06-27 9:22 AM
Show a screenshot after trying to connect with STM32CubeProgrammer.
2025-06-30 1:48 PM
2025-06-30 3:18 PM
Voltage is there. ST-Link programmer is there.
If it can't connect, a few things could be the issue:
If it has never worked, might also want to check orientation of chip and workmanship of solder joints.
2025-07-01 12:04 AM
Hello @MRuhe.1 ,
Please check this article which describes tips to fix such errors:
How to solve connection errors when connecting and programming the STM32 target board
2025-12-08 5:07 AM
Thanks to all. The issue is resolved.