cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F413 Discovery: many errors trying to debug using Eclipse with OpenOCD

isav
Associate

Sorry if this is extremely basic, as part of our program we had to install(?) RTOS on our boards to do some of the labs, but we had to reinstall ST-Link after. Now the board refuses to debug. I'm getting these logs:

xPack Open On-Chip Debugger 0.12.0+dev-01850-geb6f2745b-dirty (2025-02-07-10:08)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

DEPRECATED! use 'gdb port', not 'gdb_port'

DEPRECATED! use 'telnet port', not 'telnet_port'

DEPRECATED! use 'tcl port' not 'tcl_port'

Info : auto-selecting first available session transport "dapdirect_swd". To override use 'transport select <transport>'.

adapter speed: 100 kHz

Started by GNU MCU Eclipse

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V2J45M31 (API v2) VID:PID 0483:374B

Info : Target voltage: 3.217255

Error: Unable to set adapter speed

Info : clock speed 100 kHz

Error: SRST error

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x2ba01477

Error: Fail reading CTRL/STAT register. Force reconnect

Error: [stm32f4x.cpu] Examination failed

Warn : target stm32f4x.cpu examination failed

Info : [stm32f4x.cpu] starting gdb server on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Error: Target not examined yet

Error: [stm32f4x.cpu] Execution of event gdb-attach failed:

 

Error: Target not examined yet

Error: auto_probe failed

Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.

Error: attempted 'gdb' connection rejected

shutdown command invoked

Error in final launch sequence

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

Remote communication error. Target disconnected: error while reading: Connection reset by peer.

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

Remote communication error. Target disconnected: error while reading: Connection reset by peer.

Remote communication error. Target disconnected: error while reading: Connection reset by peer.

 

 

3 REPLIES 3
Pavel A.
Super User

Started by GNU MCU Eclipse

It looks like you're not using CubeIDE (which includes the proper version of OpenOCD).

 

Ozone
Principal III

I tend to agree to Pavel A.
It looks like some issue with the OpenOCD version.

I don't have experience with MCU Eclipse, although I tried it years ago.
OTOH, I recently flashed NuttX firmware to some STM32 boards under Linux, using OpenOCD, which worked well.

Perhaps you could try to 'convert' the ST-Link into a JLink with the firmware available on Segger's website, assuming MCU Eclipse supports JLink debug pods.
This step is reversible, by the way.

Andrew Neil
Super User

I also don't have recent experience with MCU Eclipse but, years ago, did manage to get it to work with ST-Links - both genuine and "clones".

It was a bit of a faff.

One of the key advantages of STM32CubeIDE is that ST have done all that faff for you - as @Pavel A. suggests.

Note that STM32CubeIDE is Eclipse.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.