2014-07-20 6:56 AM
Hi,
When I make Project, generate code, open Project in MDK, Close NKD, Change Project, generate again, open MDK,....... several times then following happens: 1.) every 2,3,4th times, when I build all of MDK Project, I get following message: ControllerV2 Configuration\ControllerV2 Configuration.sct(7): error: L6236E: No section matches selector - no section to be FIRST/LAST. Keil says that this means that there is no main function available. How ca this happen? 2.) Every time I generate the Project in CubeMX then 3 new lines added to my include path in C/C++ configuration. So after 5 time generate, I have ~20 entries in C/C++ include path in the Project configuration. How can I fix that without every time to delete all addede entries. 3.) After every generate, a lot of entries in my MDK Project configuration are changed. For example my Quarz freqencies, type of Emulator, type of Debug,.... How can I hint the CubeMX from changing These values? I Need o say that this tool is the best tool I had in the last 5 years. It helps me to save huge amount of time to configure the contoller for the required Outputs. Thanks a lot #keil2014-07-21 7:06 AM
2014-07-31 12:14 PM
Hi,
See attached the sample project. When you look at the compiling options in C/C++ section/Include path, you see a lot of similar include paths. If you generate 100 times the files, this will get huge size. ________________ Attachments : Test1.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzQF&d=%2Fa%2F0X0000000bLi%2F5d7DtAPwTJp8RpVsJQJkFvxY_hvPKgS45XXk7cRlOfk&asPdf=false2014-08-14 11:51 AM
Maybe this asm file is missing: startup_stm32fxxxxx.s
It's located at ..\Drivers\CMSIS\Device\ST\STM32F2xx\Source\Templates\armit's inside your project folder created by STM32CubeMX.Isaque2014-08-14 2:02 PM
Hi,
The problem is that every second generate this will happen. I have absolutley no idea why.Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.