cancel
Showing results for 
Search instead for 
Did you mean: 

Start the project with STM32F769I-EVAL board using Atollic TrueStudio and STM32CubeMX 5.1.0

RGate.15
Associate

I have a STM32F769I-EVAL board and am using Atollc TrueStudio development tools and STM32CubeMX 5.1.0 to start the project.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello,

Do you face any problem to start your project?

The STM32CubeF7 firmware package provides a rich set of examples and applications that helps you:

STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I_EVAL

Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
RGate.15
Associate

​I was trying to copy information into my original post when it sent the post before I was ready.  I have a project and it compiles with the Atollic tool set.  When I go to debug it, I get the following message:

Failed to execute MI command:

-file-exec-and-symbols C:/Users/rgate/Desktop/Third/Third.elf.launch

Error message from debugger back end:

"C:/Users/rgate/Desktop/Third/Third.elf.launch": not in executable format: File format not recognized

The board had been used for a previous project and so the demo software is not installed in it.