Skip to main content
MDe L.3
Associate II
August 10, 2021
Solved

SMT32 Embedded target: error in Simulink. How to fix "Support for the RTW.HWDeviceRegistry class has been removed."

  • August 10, 2021
  • 1 reply
  • 1782 views

Hi, I am trying to build a Simulink model by using the STM32 Embedded Target. By following the instructions provided in the manual, I added the path in Matlab, and, in Simulink, I went to " Configuration Parameters --> Code Generation " and selected the "System target file" stm32.tlc from the list. However, I get several warnings/errors.

1 ) Warning: An error occurred while evaluating "loc_register_device" in

"C:\MATLAB\STM32-MAT\STM32\script\sl_customization.p": Support for the RTW.HWDeviceRegistry class has been removed.

2) Warning: Error executing the PostApplyCallback of the target "stm32.tlc":

Path not found ===> STM32CubeMx not installed or modify "STM32CubeMx installation path"

field.

The sl_customization.p is a non-readable file. I have installed the STM32CubeMx and also already tried and it works. Any ideas on how to solve these issues?

Best

This topic has been closed for replies.
Best answer by MDe L.3

I found that I need to go to "Configuration Parameters" and select "STM32 Options" in the Code Generation. There, I ticked "STM32CubeMx Path update". Now it works.

1 reply

MDe L.3
MDe L.3AuthorBest answer
Associate II
August 10, 2021

I found that I need to go to "Configuration Parameters" and select "STM32 Options" in the Code Generation. There, I ticked "STM32CubeMx Path update". Now it works.