2024-02-04 2:28 AM
Hi,
I want to program my STM32H753ZI Nucleo board with Simulink. I successfully programmed it to blink an LED. However, I get the following error when I try to enable a timer (for PWM, or Encoder).
C:/ProgramData/MATLAB/SupportPackages/R2023b/toolbox/shared/supportpackages/stm32/src/rtiostream_serial.c:10:10: fatal error: rtiostream.h: No such file or directory
10 | #include "rtiostream.h"
| ^~~~~~~~~~~~~~
compilation terminated.
gmake: *** [rtiostream_serial.o] Error 1
I have tried this with both CubeMx 6.4 and 6.10 (Matlab has recommended to use CubeMx 6.4.).
I have also tried the STM32F446RE Nucleo board and the same error emerged.
Any suggestions to solve this problem are highly appreciated.
Thanks
2025-10-12 11:59 AM
Oh okay, will have another scan through each of the folders in the path and see if I spot anything out of place!
I'll update if you have saved my life once I've done it
2025-10-12 2:53 PM
I just realised after all this time that your problem was slightly different from the initial that started this thread, I have the lack of "rtiostream.h" issue originally presented by hsafamehr.
Sorry for wasting your time on this matter, hopefully I can find someone as helpful with you that has experience with my issue.
2025-10-12 2:55 PM
Hi there,
I'm having this issue also. When I manually added the header files requested to the path from another are in MATLAB, it just led to further errors rising due to a lack of functions being defined in this alternate header file.
Also, should I use the latest version of CubeMX, Matlab gets quite unhappy during ths installation process and breaks stuff further.
Do you have any advice?