2020-07-22 2:12 AM
I simply want to read A0 analog pin through terminal on Truestudio however after weeks of trying I need help. My step-by-step guide on what I have done is below:
In STM32CubeMX I initialised all peripherals.
I set PA0 as ADC1_IN5. I initialised ADC1_IN5 as single ended.
I set PA10 as GPIO_Output.
I enable USART2 as asynchronous.
I export to truestudio.
The code I add is as follows:
#include <string.h>
#include <stdio.h>
/* USER CODE BEGIN 1 */
uint16_t raw;
char msg[10];
/* USER CODE END 1 */
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_SET);
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
raw = HAL_ADC_GetValue(&hadc1);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, GPIO_PIN_RESET);
sprintf(msg, "%hu\r\n", raw);
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
/* USER CODE BEGIN 3 */
HAL_Delay(1);
/* USER CODE BEGIN 3 */
}
There are no error messages with this code. However, nothing prints on the terminal. Any explanations would be greatly appreciated :) I am new to TrueStudio.
Have a nice day!
2020-07-22 3:45 AM
Hello,
Try to add this function to your code :
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
/***********************************************************************/
PUTCHAR_PROTOTYPE
{
/* Place your implementation of fputc here */
/* e.g. write a character to the terminale and Loop until the end of transmission */
HAL_UART_Transmit(&UARTHandle, (uint8_t *)&ch, 1, 0xFFFF);
return ch;
}Best Regards,
Mohamed Aymen.
2020-07-22 4:51 AM
Hello Mohamed,
Thank you very much for the response.
I have not used the 'fputc' function before and I have just watched some videos to try and understand.
I am not sure how to use this method to read the analog pin continuously? It seems as though it saves the data to a file (though this will be useful in future). How do I replace the character with A0 and loop continuously?
kind regards,
Jacob