2018-05-24 11:06 AM
Hi there,
I've been working with eclipse-workbench for half a year now, creating my projects from STM32Cube tab inside eclipse and exporting them to eclipse. Until now everything was working fine, I could edit the .ioc file and update the configuration to eclipse without any problem.
Don't know why, but since today, when I try to create a new project or edit the ones already were working, I have the following error:
''Please install SW4STM32 toolchain to open the project.
Or associate the file type of the project with you Toolchain in System Default Program Settings''
Any clue how to solve it?
Thanks
#stm32 #workbench #error #eclipseSolved! Go to Solution.
2018-05-27 8:40 AM
Hi,
I installed latest version of CUBE with no succeed. I've installed “System Workbench for STM32� again, keeping the previous installation (now I have 2 Workbenchs) and both are working now, so I'm going to keep it.
2018-05-25 2:56 AM
Hi
maniljo
,Do you face the issue with the latest version of CUBEMX (4.1)?
-Nesrine-
2018-05-25 5:17 AM
Hi
ELMHIRI.Syrine
Thanks for you answer. Right now I'm not in front of my computer, but pretty sure is above 4.
I've been using Workbench/CUBEMX oftenly for almost a year and it worked perfectly.
Quite extrange problem since it is reproduced on the projects that previously worked fine.
2018-05-25 5:56 AM
Hi
maniljo
,Please try to use the latest version and tel us if the issue still again.
-Nesrine-
2018-05-27 8:40 AM
Hi,
I installed latest version of CUBE with no succeed. I've installed “System Workbench for STM32� again, keeping the previous installation (now I have 2 Workbenchs) and both are working now, so I'm going to keep it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.