2026-06-05 4:36 AM
Hi everyone,
I have a schematic using the Realtek RTL8211F-CG Gigabit Ethernet PHY and I want to connect it directly to an STM32H7 microcontroller for Ethernet communication.
My questions are:
Any help or experience is appreciated. Thanks!
Solved! Go to Solution.
2026-06-05 4:59 AM
Hello,
A question that you need to address to Realtek
2026-06-05 4:59 AM
Hello,
A question that you need to address to Realtek
2026-06-05 5:02 AM
@Meer wrote:2. The RTL8211F-CG datasheet mentions it can operate at 10/100 Mbps as well — but does it support a true RMII mode that the STM32H7 MAC can talk to?
You would have to ask RealTek that.
@Meer wrote:4. If this is not possible at all, what is the simplest/cheapest alternative 10/100 PHY that works reliably with STM32H7 in RMII mode?
Simplest, surely, would be to use whatever the ST boards use?
2026-06-05 5:55 AM
Thanks for your comment. I will asked to RealTek
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.