Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Migrating code from IAR to GCC: __no_init, __ramfunc

Hey,I am trying to modify some compiler/linker directives from IAR to GCC. I think I already managed to solve the first two obstacles:1 - In order to not initialize a variable saved in some register:static volatile __no_init uint32_t SystemInfoFlags;...

AZube.2 by Associate III
  • 3527 Views
  • 1 replies
  • 0 kudos

Resolved! How to install Atollic TRUEStudio on Linux?

Hello, I have installed previous version of Atollic (< 9.3) before following the official installation guide, but now it seems to be outdated since the downloadable file isn't a .tar.gz file anymore, but now just a .gz file. I am using EndeavourOS L...

ARied.1 by Associate II
  • 3641 Views
  • 7 replies
  • 0 kudos

Resolved! Arduino milis() function stm32f103xx

I am trying to port some Arduino library to stm32. In Arduino, millis() returns the number of milliseconds since boot. Is there an equivalent function in stm32? I am using stm32f103 MCU.

Bicer by Associate II
  • 6012 Views
  • 6 replies
  • 1 kudos

Hi, set stm32H750 tim, Error in 'deviceManage/Function-Call Subsystem/Timers': Initialization commands cannot be evaluated. TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 is use

Hi, set  stm32H750 tim, Error in 'deviceManage/Function-Call Subsystem/Timers': Initialization commands cannot be evaluated. TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 i...

0690X00000D8vuiQAB.png
lling.1 by Associate II
  • 3863 Views
  • 15 replies
  • 0 kudos