Skip to main content
lijokuriakose
Associate
September 11, 2006
Question

XASC Problem

  • September 11, 2006
  • 3 replies
  • 854 views
Posted on September 11, 2006 at 06:26

XASC Problem

This topic has been closed for replies.

3 replies

lijokuriakose
Associate
September 8, 2006
Posted on September 08, 2006 at 10:05

Hello,

I can't transmit any data(XASC)...am using keil compiler

Download & checking in evaluation board

Even i have chenged in start up settings ( SYSCON =0x0004,XPERCON =0x0080)

pls find the below code and help me

=============================================================

#include ''ST10F276.H''

sbit DP2_0 = DP2^0;

sbit P2_0 = P2^0;

void main()

{

int i,j,k;

DP2_0 =1;

P2_0 =1;

//SYSCON =0x0004;

//XPERCON =0x0080;

//P8 |= 0x0080;

//DP8 |= 0x0080;

XS1PORT = 0x0018;

XS1BG = 0x81u; // 9600

XS1CON = 0x8011;

XIR1CLR=0xFFFF; // XIR1SEL register clear

XIR1SET=0x4000; // Set bit 15 of XIR1SEL > XASC Transmit Int. connected to X-Periph. Interrupt Vector 1, XP1INT

XP1IC=0x0045; // xxxx.xxxx.x100.0101 XP1INT (XSSC Transmit) Int. enable, ILVL=1, GLVL=1 XP2IC = 0x2E; // ILVL = 11 and Group level 2

IEN = 1;

while(1)

{

P2_0 =~P2_0; //toggle pin

XS1TBUF='A'; // Trying to send continuous data

for(i=0;i<=65534;i++);

for(j=0;j<=65534;j++);

for(k=0;k<=65534;k++);

}

}

void XPeriph_Int1( void ) interrupt 0x41 // XSSC Tx Interrupt

{

}

============================================================

i am trying to send 'A' continuously

But its not working

Or anybody can send a sample code to ''leelijo@rediffmail.com''

Regards,

Vinu

najoua
Associate
September 8, 2006
Posted on September 08, 2006 at 11:12

Hello,

I noticed a mistake in your configuration (XPERCON =0x0080):

In order to to be able to use X-Bus peripherals, XPEN bit in SYSCON register and the peripheral enable bit (XASCEN in our case) & XMISCEN bit in XPERCON register must be set.

So, could you please set XMISCEN bit in XPERCON register and let me know how it goes?

Please refer to the discussion forum on the follwowing link:

http://www.stmcu.com/forums-cat-2864-5.html

Regards,

Najoua.

[ This message was edited by: Najoua on 08-09-2006 15:01 ]

lijokuriakose
Associate
September 11, 2006
Posted on September 11, 2006 at 06:26

hello,

yaa its working.. thanks

Regards,

Vinu :p