cancel
Showing results for 
Search instead for 
Did you mean: 

using ST7F521 with 3.3V devices

dominique23
Associate II
Posted on January 07, 2003 at 11:04

using ST7F521 with 3.3V devices

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
dominique23
Associate II
Posted on January 07, 2003 at 05:45

I would like to use ST7F521 with a 3.3V Fpga, I have been said that the 2 additionnal port (G and H) of the 80 pins version are TTL whereas the port in the 64pin version are all in true cmos level (3.5v min for H level).

I want to have confirmation of this information.

Thanks.
sjo
Associate II
Posted on January 07, 2003 at 08:16

The additional ports are TTL but your main concern would be that the newer revision silicon (datasheet v1.6) supports only 3.8-5.5v operating conditions.

Regards

Spen
dominique23
Associate II
Posted on January 07, 2003 at 09:41

thanks you very much but where can I find this version of the datasheet, I don't find it on this site...

simms
Associate II
Posted on January 07, 2003 at 11:04

should be accessible from this site by selecting ST72521 product from the home page

try this link too, if it helps...

http://us.st.com/stonline/books/pdf/docs/7601.pdf