cancel
Showing results for 
Search instead for 
Did you mean: 

USBLC6-4SC6 for EFT and lightning protection

gordon239955
Associate

Hi,

Can USBLC6-4SC6 be used to protect an IO from EFT (IEC 61000-4-4) and lightning (IEC 61000-4-5)? I do not see any specification for these standards? Thanks.

Regards

Gordon

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FGUIT
ST Employee

Hi,

Regarding IEC 61000-4-5, USBLC6-4SC6 is able to withstand 5A with a 8/20 µs surge, this is specified on the Table 2.

Best regards.

Fabrice.