2026-05-27 11:33 PM - last edited on 2026-05-28 12:06 AM by Andrew Neil
A P-channel MOSFET is currently used for switching the solenoid.
Case 1:
Is it possible for the MOSFET to fail?
Case 2:
If the MOSFET fails, will it become an open circuit or a short circuit?
Case 3:
If the MOSFET fails in short-circuit condition, how can the circuit be protected
2026-05-27 11:56 PM
Welcome @jalathar, to the community!
Your questions are questions about the fundamentals of electrical engineering and sound like exam questions from schools.
Is there a specific reason why you’re asking this in a forum for STMicroelectronics devices?
Regards
/Peter
2026-05-28 12:37 AM
In case P Channel MOSFET get fail it become open circuit or short circuit (soruce and Drain)?
2026-05-28 1:04 AM
A fixed probability for the two cases cannot be stated without specific data. A short circuit between D-S is usually more likely in the event of overload, while an open-circuit fault is more likely if e.g. connection wires, metallisation or mechanical structures fail. The exact cause depends greatly on what the overload looks like.
In short, there can be no general answer to your question.
Regards
/Peter
2026-05-28 1:07 AM
My Use of MOSFET is switch the startrer motor solenoid
If possible shortcircuit occur in source to drain ?
2026-05-28 1:24 AM
Yes.
2026-05-28 1:25 AM
How to protect the short circuit