cancel
Showing results for 
Search instead for 
Did you mean: 

Uart driver code for str912fw44

girija_79
Associate
Posted on November 23, 2006 at 02:37

Uart driver code for str912fw44

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
girija_79
Associate
Posted on May 17, 2011 at 11:31

Hi everybody!

i am writing driver code for uart(of str912fw44) i am very new to this processor i was working with LPC21xx from past 2 weeks i am into this st and i have my deadline nearing please help me by telling what is wrong in my code and i havenot found datasheet for str912fw44 can anyone help me with that and help with my driver code

void main()

{

uint8_t a[5];

UART_InitTypeDef UART_InitStructure;

void SCU_Configuration(void);

void GPIO_Configuration(void);

#ifdef DEBUG

debug();

#endif

/* Configure the system clocks */

SCU_Configuration();

/* Configure the GPIO ports */

GPIO_Configuration();

UART_InitStructure.UART_WordLength = UART_WordLength_7D;

UART_InitStructure.UART_StopBits = UART_StopBits_2;

UART_InitStructure.UART_Parity = UART_Parity_No ;

UART_InitStructure.UART_BaudRate = 9600;

UART_InitStructure.UART_HardwareFlowControl = UART_HardwareFlowControl_RTS_CTS;

UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx;

UART_InitStructure.UART_FIFO = UART_FIFO_Enable;

UART_InitStructure.UART_TxFIFOLevel = UART_FIFOLevel_1_2; /* FIFO size 16 bytes, FIFO level 8 bytes */

UART_InitStructure.UART_RxFIFOLevel = UART_FIFOLevel_1_2; /* FIFO size 16 bytes, FIFO level 8 bytes */

UART_DeInit(UART0);

UART_Init(UART0, &UART_InitStructure);

/* Enable the UART0 */

UART_Cmd(UART0, ENABLE);

UART_ReceiveData(UART0, &a[0] );

UART_SendData(UART0, a[0]);

}

void SCU_Configuration(void)

{

/* Enable the UART0 Clock */

SCU_APBPeriphClockConfig(__UART0, ENABLE);

/* Enable the GPIO2 Clock */

SCU_APBPeriphClockConfig(__GPIO2, ENABLE);

/* Enable the GPIO3 Clock */

SCU_APBPeriphClockConfig(__GPIO3, ENABLE);

/* Enable the GPIO5 Clock */

SCU_APBPeriphClockConfig(__GPIO5, ENABLE);

}

void GPIO_Configuration(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

/*Configure UART0_CTS P2.0*/

GPIO_DeInit(GPIO2);

/*After DeInit function P2.0 = UART0_CTS (defaut configuration)*/

GPIO_DeInit(GPIO5);

/*Gonfigure UART0_Rx pin GPIO5.1*/

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1 ;

GPIO_Init (GPIO5, &GPIO_InitStructure);

GPIO_DeInit(GPIO3);

/*Gonfigure UART0_Tx pin GPIO3.4*/

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3 ;

GPIO_Init (GPIO3, &GPIO_InitStructure);

/*Gonfigure UART0_RTS pin GPIO3.3*/

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3 ;

GPIO_Init (GPIO3, &GPIO_InitStructure);

}

void UART_SendData(UART_TypeDef* UARTx, uint8_t Data)

{

//while ((UARTx->FR & 0x0060)==0);

// UARTx->FR |= UART_Enable_Mask;

/* Transmit one byte */

UARTx->DR = Data;

}

/*******************************************************************************

* Function Name : UART_ReceiveData

* Description : Returns the most recent received Byte by the UARTx peripheral.

* Input : UARTx: where x can be 0,1 or 2 to select the UART peripheral.

* Output : None

* Return : The received data

*******************************************************************************/

uint8_t UART_ReceiveData(UART_TypeDef* UARTx,uint8_t *pdata )

{

//while(!(UARTx->DR & 0x00ff)==0);

/* Receive one byte */

*pdata = UARTx->DR;

// return ((uint8_t)UARTx->DR);

return 0;

}

please see whether my send data and receive data modules are correct

Thanking all of u all in advance please do help me since i am very new to this microcontroller and this field tooo ,