cancel
Showing results for 
Search instead for 
Did you mean: 

transfer *.hex / *.bin file to upsd

babidesai123
Associate II
Posted on May 13, 2003 at 08:40

transfer *.hex / *.bin file to upsd

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
babidesai123
Associate II
Posted on May 06, 2003 at 07:43

Hello,

I would like to transfer hex or bin file to PC comm port

IF anyone has some example code for the same.???

stephanie
Associate II
Posted on May 09, 2003 at 12:23

Be more precise: do you want to send your hex or bin file from a ST7 to the PC? If yes, this can be done through the SCI communication peripheral for instance. You will find some application notes giving code on this site.

itsmejatinus
Associate II
Posted on May 13, 2003 at 08:40

One Application Note is present i.e. AN 969 (SCI communication between ST7 and PC). You can download it from the same site.