cancel
Showing results for 
Search instead for 
Did you mean: 

Timer 0 IRQ entered 2 times

mgerkens9
Associate II
Posted on May 09, 2007 at 10:33

Timer 0 IRQ entered 2 times

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mgerkens9
Associate II
Posted on May 17, 2011 at 09:43

Hi all,

i have the following problem:

I run the timer 0 in Output Compare 1 Mode with the interrupt enabled cause i need an 1ms Clock. Now, when an Interrupt occurs, i toggle an LED and i see on my Scope, that the IRQ-Routine is entered 2 times directley next to each other. I have attached my Source-Code.

Thanks for Help :)

And i also work not with the complicated Libs from ST, i directly uses the Register !!!

Michi

mgerkens9
Associate II
Posted on May 17, 2011 at 09:43

Sorry, this is the Wrong Forum, i need the str9 forum . . .