Skip to main content
mariusz2
Associate III
January 23, 2009
Question

timer in str911fm44

  • January 23, 2009
  • 8 replies
  • 1759 views
Posted on January 23, 2009 at 18:35

timer in str911fm44

This topic has been closed for replies.

8 replies

markmcwired9
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:42

Hi MariuszS,

I use this code to generate a 10mSec interrupt:

>>>>>> This code goes in the setup part:

// TIM0 Structure Initialization ---------------------------------------------

/* Timer calculation:

Period = (t * fPCLK / tPRESC) - 5

Where:

t = Desired output compare period (seconds)

fPCLK = Internal clock frequency

tPRESC = Timer clock prescaler

Ex: Period = (0.01 * 48Mhz / 256) - 5 = 0x74E

*/

TIM_StructInit(&TIM_InitStructure);

TIM_InitStructure.TIM_Mode = TIM_PWM;

TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB;

TIM_InitStructure.TIM_Prescaler = 0xFF;

TIM_InitStructure.TIM_Pulse_Level_1 = TIM_HIGH;

TIM_InitStructure.TIM_Period_Level = TIM_LOW;

TIM_InitStructure.TIM_Pulse_Length_1 = 0xFF;

TIM_InitStructure.TIM_Full_Period = 0x74E; //0xFFF max value for 22mSec

TIM_DeInit(TIM0);

TIM_Init (TIM0, &TIM_InitStructure);

TIM_ITConfig(TIM0, TIM_IT_TO, ENABLE); // Enable the Timer Overflow interrupt

TIM_CounterCmd(TIM0, TIM_START); // Start the Timer0 counter

// VIC configuration ---------------------------------------------------------

VIC_DeInit();

VIC_Config(TIM0_ITLine, VIC_IRQ, 4);

VIC_ITCmd(TIM0_ITLine, ENABLE);

>>>>>> This code goes in the ''91x_it.c'' file:

void TIM0_IRQHandler(void)

{

TIM0_IRQHandlerInvoked();

}

>>>>>> This code goes in the subroutine called by the interrupt:

/*******************************************************************************

* Function Name : TIM0_IRQHandlerInvoked

* Description : this routine is invoked when the Timer0 has generated an

* interrupt

*******************************************************************************/

void TIM0_IRQHandlerInvoked(void)

{

TIM_ClearFlag(TIM0, TIM_FLAG_TO); //Clear the TIM_TO flag for the next interrupt

if(pulse)

{

GPIO_WriteBit(GPIO6, GPIO_Pin_1, Bit_SET);

GPIO_WriteBit(GPIO2, GPIO_Pin_2, Bit_RESET);

pulse = 0;

}

else

{

GPIO_WriteBit(GPIO6, GPIO_Pin_1, Bit_RESET);

GPIO_WriteBit(GPIO2, GPIO_Pin_2, Bit_SET);

pulse = 1;

}

}

I just toggle Leds when the interrupt happens. I hope this will help you.

Mark

mariusz2
mariusz2Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:42

Can my help. How configure any timer, to time mensure from internal clock SCU. I need interrupt from timer, constant period without PWM, PULSE, and other hardware events. please example code

amira1
Associate
May 17, 2011
Posted on May 17, 2011 at 09:42

Hello GKruger,

Please find attached a Timer example working with fPLL=48MHz. To calculate the Timer frequency :

fTIM=fPCLK/(tPRESC*(OC2R-5))

So you will get from the example fTIM=45.8Hz.

I hope this will help,

With best regards,

mirou

gkruger
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:42

Hello,

I seem to get exactly double the period that I should. I used Mike's code as a test. And I get 20ms not 10ms.

My first thought was that my clock speed is wrong, I am running at 48MHz (SCU_PLLFactorsConfig(192, 25, 3);)

If I call SCU_GetMCLKFreqValue() I get 48000 back.

Is there anything else that I am missing?

Thanks,

Gert

mariusz2
mariusz2Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:42

Very thanks. My problem was in library functions 91x_Lib.c. Copmiler not handled:

#ifdef _TIM0

TIM0 = (TIM_TypeDef *)TIM0_BASE;

#endif /* _TIM0 */

all function ''timers'' need this registration in debug mode

Is possible use function in no debug mode? How?

boris1
Visitor II
May 17, 2011
Posted on May 17, 2011 at 09:43

2 lazycat1049:

pulse length is 0xFF because we need divide prescale value = 256. Look at Reference manual at TIM_CR2 register

(CC[7:0]: Clock Control.

These bit are written by software to select the frequency of the timer clock applied

when internal clock is selected (ECKEN=0):

00h: fPCLK / 1

01h: fPCLK / 2

...

FFh: fPCLK / 256

)null

lazycat1049
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:43

Hi,

Sorry can anybody tell mi why pulse length is 0xFF in the above code?

Thanx in advance!!

Lazycat

jtremblay
Visitor II
May 17, 2011
Posted on May 17, 2011 at 09:43

I just want to keep you informed that the formula to compute fTIM has an error. You should read fTIM = fPCLK / (tPRESC * (OCR2 + 5) ). I have tested it with my 100uS tick timer and it is very accurate.

Jim