cancel
Showing results for 
Search instead for 
Did you mean: 

Support ST7

asherman
Associate II
Posted on January 20, 2003 at 12:39

Support ST7

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
asherman
Associate II
Posted on January 20, 2003 at 09:45

When i am working with the ST7 in ICP feature with the EPB from STM . I need to put VDD to my board or the 10pin connector with the ICP function includes the VDD ?

Posted on January 20, 2003 at 12:39

You always need to power up your target board when using an EPB in ICP mode : the EPB uses the application VDD as voltage reference signal to provide the right voltage level on the ICCCLK and ICCDATA pins. The EPB Vdd pin has not been designed to power user's application boards.

Take care,

Jojo