cancel
Showing results for 
Search instead for 
Did you mean: 

STR9 Network bootloader developed

dibacco2
Associate II
Posted on August 22, 2007 at 06:48

STR9 Network bootloader developed

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
dibacco2
Associate II
Posted on May 17, 2011 at 09:45

Hi,

I attached a CrossWorks 1.7 project of a bootloader to load in Bank1 of STR9 that receives a file from network using uIP and writes it to Bank 0. Everything is working fine but when jumping to Bank 0, it doesn't work.

A user application has to open a TCP connection to IP 192.168.0.11 and port 1234 and download an header with 4 magic bytes, 4 bytes representing length of file and then the file itself. I verified that the file is copied to flash of Bank 0. Anyone could cooperate with me to give an hint why the final jump is not working?